SDK 1.3 - KV10Z128 issue with IAR7.60.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK 1.3 - KV10Z128 issue with IAR7.60.1

926件の閲覧回数
guenter_loettrich
NXP Employee
NXP Employee

Hi all,

customer discovered an issue with the "Hello World" example for the KV10Z128 in SDK1.3.

When working with the standard settings of the project for KV10Z128 then the flashloader "KVxx128K.flash" is used and causes an abort of the flash process.

However when uisng the KV11 flashloader "KV11128K.flash" for the KV10Z128 project then everything works fine.

File compare shows difference in the <block> section for both devices although they should have identical settings.

(See file comparison:)



   
Please follow up with SDK1.3 responsible people and IAR if necessary to get that corrected.
 

br

Guenter

ラベル(1)
0 件の賞賛
返信
1 返信

742件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Guenter Loettrich​,

thank you very much for your feedback!

I reported the issue to our team, you can find it here http://sw-jira.freescale.net/browse/KPSDK-10876

Have a great day!

Best Regards,

Iva