SDK 1.3 - KV10Z128 issue with IAR7.60.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK 1.3 - KV10Z128 issue with IAR7.60.1

923 Views
guenter_loettrich
NXP Employee
NXP Employee

Hi all,

customer discovered an issue with the "Hello World" example for the KV10Z128 in SDK1.3.

When working with the standard settings of the project for KV10Z128 then the flashloader "KVxx128K.flash" is used and causes an abort of the flash process.

However when uisng the KV11 flashloader "KV11128K.flash" for the KV10Z128 project then everything works fine.

File compare shows difference in the <block> section for both devices although they should have identical settings.

(See file comparison:)



   
Please follow up with SDK1.3 responsible people and IAR if necessary to get that corrected.
 

br

Guenter

Labels (1)
0 Kudos
Reply
1 Reply

739 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Guenter Loettrich​,

thank you very much for your feedback!

I reported the issue to our team, you can find it here http://sw-jira.freescale.net/browse/KPSDK-10876

Have a great day!

Best Regards,

Iva