SDK_1.3_FRDM-KL03Z debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK_1.3_FRDM-KL03Z debug

3,302件の閲覧回数
zhiyuwang
Contributor I

Does SDK_1.3_FRDM-KL03Z support debug?

I down load SDK_1.3_FRDM-KL03Z and build successfully. i try to do online debug. but "download" menu is disabled?

 

143912_143912.pngpastedImage_0.png

 

Best regards,

ZY

ラベル(1)
タグ(1)
0 件の賞賛
返信
6 返答(返信)

3,157件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi ZY,

The "Hello world " is a simple project , if you do not want to use KSDK, you can

delete the more codes about KSDK .

And you can also  create one new project refer to the EW_GettingStarted.ENU.pdf  for the part

"Creating an application project " .

Hope it helps

Alice

0 件の賞賛
返信

3,157件の閲覧回数
zhiyuwang
Contributor I

Hi Alice,

For the project in “SDK_1.3_FRDM-KL03Z” doesn`t support debug. I just want an blank project base on “MKL03Z32VFG4” to verify debug function.

Best Regards,

Zhiyu Wang

0 件の賞賛
返信

3,157件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Oh Zhiyu,

The KSDK1.3_lib doesn't support debug , for your project, please click the proejct of "lpuart_...",

then debug it .

pastedImage_0.png

If still can not, please take a screenshot step by step about how did you operate , and

show me you have select the project you want to debug , not the lib .

BR

Alice

0 件の賞賛
返信

3,157件の閲覧回数
zhiyuwang
Contributor I

Hi Alice,

Would you like give me a blank project just as “hello world”
base on “MKL03Z32VFG4” which supports debug?

Best Regards,

ZY

0 件の賞賛
返信

3,157件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Zhiyu,

please select the project , not the KSDK lib , then download , it can work well :

pastedImage_0.png

pastedImage_1.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,157件の閲覧回数
zhiyuwang
Contributor I

Hi Alice,

Would you like give me a blank project just as “hello world” base on “MKL03Z32VFG4” which supports debug?

Best Regards,

Zhiyu Wang

0 件の賞賛
返信