SDHC 4bit bus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDHC 4bit bus

3,101 次查看
adyr
Contributor V

Hi,

 

I think there is a shortfall in the KSDK / Processor Expert SDHC component or driver. Not sure if it is a PEx or KSDK problem so this might be in the wrong place.

 

I set the bus width to 4 bits in the Init Configurations tab of the fsl_sdhc component but it has no effect on the driver.

It creates "sdhc_buswidth_t fsl_sdhc1_busWidth0 = kSdhcBusWidth4Bit;" in fsl_sdhc1.c but that is never used and SDHC_DRV_Init has the line SDHC_DRV_SetBusWidth(instance, kSdhcBusWidth1Bit);.

 

Best regards,

Adrian.

标签 (1)
6 回复数

2,801 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Adrian,

Thank you very much for your focus on Freescale Kinetis product. I'm glad to provide service for you.

I was wondering if you can share your project, then I can check this issue.

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,801 次查看
adyr
Contributor V

Hi Ping,

I can't see a way to upload on here so I have replied to your email with the project as an attachment.

Basically the project is just a start up using PEx with the KSDK 1.1 and targeted at the IAR compiler. I then added and configured the fsl_sdcard component and then initialise it from a task.

Best regards,

Adrian

0 项奖励
回复

2,801 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Adrian,

Thank for your sharing and I'll check the attachment ASAP
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,801 次查看
adyr
Contributor V

Hi,

The FatFS implementation in KSDK 1.2 is now setting the 4 bit mode OK.

Does anyone know if future versions of FatFS will use the fsl_sdcard Pex component?

Adding the component in KDS does help as it ensures the pins and interrupts are setup correctly but it seems the FatFS fsl_sd_disk.c uses it's own instance of the configuration + #defines for card detection etc.

Best regards,

Adrian.

0 项奖励
回复

2,801 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Adrian,

We've also not had some information about the new feature of the updating SDK now and I'll inform you ASAP if I confirm it.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,800 次查看
adyr
Contributor V

Hi Ping,

I’m not sure how to upload on the forum so hopefully you will get the attached project.

I have started to try and integrate the KSDK fatfs into the project since my post so not sure if it will still produce a working code. I can’t find any documentation for that so it is trial and mainly error.

I also appreciate that the fatfs doesn’t use the PEx information at all.

Best regards,

Adrian.

0 项奖励
回复