RTC is inaccurate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,766件の閲覧回数
joebirch
Contributor III

The RTC is about .02% off (11 secs after 15hrs)

 

I am using the KSDK2.0 rtc_func demo ("C:\Freescale\KSDK_2.0\boards\frdmk22f\demo_apps\rtc_func").

I have tried it on 2 different FRDM-K22F eval boards

 

Board 1: 11 secs fast after 15.5 hrs

Board 2: 7 secs after 15hrs,  22 secs after 40hrs

 

The FRDM-K22F BOM shows the osc is 20PPM

 

Am I doing something wrong?

I know the RTC can be adjusted but it is unacceptable to have to customize this for each board.

 

Please help

 

Joe

ラベル(1)
0 件の賞賛
返信
1 解決策
1,537件の閲覧回数
joebirch
Contributor III

Iva

I am using the FRDM-K22 board and the the KSDK2.0 rtc_func demo ("C:\Freescale\KSDK_2.0\boards\frdmk22f\demo_apps\rtc_func").

This uses the eternal 32.768k osc.

But maybe the osc is not 20PPM as advertised.

I realize this is not a KSDK topic so I will mark this as corrected.

Thanks

Joe

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,537件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi joe birch​,

please use external clk for RTC because internal oscillator is not very accurate.

You can trim accuracy by using external capacitors.

I hope this helps you.

Have a nice day.

Iva

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,538件の閲覧回数
joebirch
Contributor III

Iva

I am using the FRDM-K22 board and the the KSDK2.0 rtc_func demo ("C:\Freescale\KSDK_2.0\boards\frdmk22f\demo_apps\rtc_func").

This uses the eternal 32.768k osc.

But maybe the osc is not 20PPM as advertised.

I realize this is not a KSDK topic so I will mark this as corrected.

Thanks

Joe

0 件の賞賛
返信