RNDIS driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,041件の閲覧回数
joevignola
Contributor III

The KSDK 2.0 USB documentation (USB Stack Device Reference Manual) has information about an USB CDC RNDIS driver in section 3.6.3 but I can not find it in the KSDK source files.

 

Please help

 

Thanks,

 

Joe.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
3,631件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Joe.

The example which demonstrates the RNDIS driver hasn’t been present in a formal release yet.

However, such example is on the schedule of release 5 , which would be released in August.

Have a great day.

Iva

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,631件の閲覧回数
joevignola
Contributor III

Iva,

Heard that the release has been delayed to the end of September.  Is it possible to get a beta release?

Joe.

0 件の賞賛
返信
3,631件の閲覧回数
mjbcswitzerland
Specialist V

Hi


Is it know whether this is also operational on a part with HS USB?

Regards

Mark

0 件の賞賛
返信
3,632件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Joe.

The example which demonstrates the RNDIS driver hasn’t been present in a formal release yet.

However, such example is on the schedule of release 5 , which would be released in August.

Have a great day.

Iva

0 件の賞賛
返信