RNDIS driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RNDIS driver

跳至解决方案
4,017 次查看
joevignola
Contributor III

The KSDK 2.0 USB documentation (USB Stack Device Reference Manual) has information about an USB CDC RNDIS driver in section 3.6.3 but I can not find it in the KSDK source files.

 

Please help

 

Thanks,

 

Joe.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
3,607 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Joe.

The example which demonstrates the RNDIS driver hasn’t been present in a formal release yet.

However, such example is on the schedule of release 5 , which would be released in August.

Have a great day.

Iva

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,607 次查看
joevignola
Contributor III

Iva,

Heard that the release has been delayed to the end of September.  Is it possible to get a beta release?

Joe.

0 项奖励
回复
3,607 次查看
mjbcswitzerland
Specialist V

Hi


Is it know whether this is also operational on a part with HS USB?

Regards

Mark

0 项奖励
回复
3,608 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Joe.

The example which demonstrates the RNDIS driver hasn’t been present in a formal release yet.

However, such example is on the schedule of release 5 , which would be released in August.

Have a great day.

Iva

0 项奖励
回复