Problems with sdcard_twrk64f120m demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with sdcard_twrk64f120m demo

ソリューションへジャンプ
3,886件の閲覧回数
tomtalkington
Contributor III

I am trying to run the sdcard_twrk64f120m demo in the MFS examples and when the SD card is inserted I see:

 

shell> Installing MFS over SD card driver...

Error while opening a:\ (UNKNOWN ERROR !!!)

 

Anyone seen / solved this before?

 

Regards,

Tom

ラベル(1)
0 件の賞賛
返信
1 解決策
3,747件の閲覧回数
tomtalkington
Contributor III

Hello Iva,

Tried several SD Cards.  None worked. Then I inspected the hardware where I found my problem.  Cold solder joints on the SD Card connector pins!  Re-soldered them and all is well.

Thank you so much for your time and help.

Best regards,

Tom

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,747件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Tom,

I will try to help you with your issue.

Please, what KSDK version do you use?

Kind Regards,

Iva

0 件の賞賛
返信
3,747件の閲覧回数
tomtalkington
Contributor III

Hi Iva,

Thanks for the help.

I am using KSDK Version 1.3.0.  TWR-K64F120M board.  IAR Embedded Workbench 7.30.1

Regards,

Tom

0 件の賞賛
返信
3,744件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Tom,

according to your error message

Error while opening a:\

it looks on problem with SD Card.

at the moment I tested the demo and on my side it works without problems.

Please, see the video which I attached you. (I skipped building project)

Please, did you try another SD Card? What file system do you use?

Best Regards,

Iva

0 件の賞賛
返信
3,748件の閲覧回数
tomtalkington
Contributor III

Hello Iva,

Tried several SD Cards.  None worked. Then I inspected the hardware where I found my problem.  Cold solder joints on the SD Card connector pins!  Re-soldered them and all is well.

Thank you so much for your time and help.

Best regards,

Tom

0 件の賞賛
返信