Power down ADC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power down ADC

1,448件の閲覧回数
tedmawson
Contributor III

I've created a project that sets up the ADC16 to read a value 4 times a second triggered by a lptmr interrupt.  I go into VLPS mode once I've done my processing for each ¼ second interval and wait for the next lptmr interrup to occur but my power drwa is still way higher than I expected and I think a big part of that is becuase the ADC is still enabled.

 

I'd like to power down the ADC when I have done with it but then power it back up each ¼ second to take my reading.  Is there a simple way to achieve this that does not involve going through all the initialization and calibration routines?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,321件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ted,

I am sorry for the delay.

I do not know the part number you are using, anyway, the ADC16 module is similar.

Regarding the ADC configuration for low power mode, I suggest you use Asynchronous clock to save power by setting ADC_CFG1[ADICLK]=2b11, while clearing the ADC_CFG2[ADCACKEN] and ADC_CFG2[ADHSC]. You can also set the ADC_CFG1[ADLPC] bit. If you set the ADLPC bit, I suppose that the ADC clock should be less than 4MHz.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信