Not UART interrupt is triggered when working Lwip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not UART interrupt is triggered when working Lwip

ソリューションへジャンプ
1,935件の閲覧回数
maksim_lipskiy
Contributor III

Hello All.
I use FRDM_K64F board and KSDK_1.0.0.
In my program is used UART_4 connected to the RS485, UART_3 connected to the USB and Lwip.
When connected to the network cable after a while stopped taking data UART_4 (RS485).

The program is part of the interrupt handler, but the function UART_HAL_GetRxDataRegFullIntCmd (baseAddr) is always false.

Thus UART is connected to the USB works correctly.

Thanks.

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,734件の閲覧回数
maksim_lipskiy
Contributor III

Thank you all very much.
Problem solved.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,735件の閲覧回数
maksim_lipskiy
Contributor III

Thank you all very much.
Problem solved.

0 件の賞賛
返信