No wsd project files in the demo folder of sdk 2.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No wsd project files in the demo folder of sdk 2.1

1,187件の閲覧回数
roymessinger
Contributor V

Hi,

I'm a newbie in the FRDM K64 board (and in ARM in particular). I've downloaded the KDS software and the SDK 2.1 file, unzipped it, followed all the instructions to load a Hello World project, but... no wsd project files are available in the demo folder.

All the tutorials I've found in NXP website points to that demo folder. What is going on?

I've downloaded IAR sdk, and in the demo folder of that zip file, they do have all the projects files of IAR, but I want to work with KDS...

Only files I have in that folder of KDS are: setting folder and .cproject & .project files. that's it.

Thanks.

ラベル(1)
1 返信

1,010件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you use IAR, you just need to double click the *.eww, the example project will be imported into the IAR, you can make it, it is okay.

If you use KDS tools, you need follow up the procedures:

1)load KDS tools, click File->import, then in the IMPORT menu, select General->Existing Project into Workspace, then click next, browse the project you want to import, it is okay.

Hope it can help you

BR

Xiangjun rong