No UART0 driver support for KL16 in KSDK 1.2.0 ??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

No UART0 driver support for KL16 in KSDK 1.2.0 ??

跳至解决方案
1,969 次查看
hengguangyang
Contributor III

Hello,

I'm working on KL16Z128 with KSDK_1.2.0 and PEx. But I can't find driver for UART0 when I config components using PEx. Who can tell me why? Is there something I missed? What's the right way to use UART0?

Thanks.

0 项奖励
回复
1 解答
1,772 次查看
hengguangyang
Contributor III

Thank you Daniel.

I got the reason now. The UART0 is seperated from UART1/2. And furtherly, the PEx component for UART0 driver is LPSCI, not UART. That confused me before.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,772 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Yang

There are two tabs for uart config. One is UART,  you can config UART1 and UART2

The other tab is specifically for uart 0, please see pictures below.

pastedImage_1.png

pastedImage_2.png

Regards

Daniel

0 项奖励
回复
1,773 次查看
hengguangyang
Contributor III

Thank you Daniel.

I got the reason now. The UART0 is seperated from UART1/2. And furtherly, the PEx component for UART0 driver is LPSCI, not UART. That confused me before.

0 项奖励
回复