MKV30F64VLH10 working in debug mode but not working after power cycle.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKV30F64VLH10 working in debug mode but not working after power cycle.

Jump to solution
3,259 Views
vaibhavsomani
Contributor II


Hi

 

I am trying to flash Freescale MKV30F64VLH10 on my board. I am flashing via PE micro Multilink Universal.
When I debug or flash via KDS3.0 and while JTAG connector is connected, my code works as defined. I am getting correct output on gpio.
But when I power off and power on the supply, I am not getting the output on gpio. And  I am getting a pulse on rest pin (looking like mcu is not getting programmed !!).

Please suggest some solution for this problem.

 

Here is the console output....

Connection from "127.0.0.1" via 127.0.0.1

Copyright 2012 P&E Microcomputer Systems,Inc.

Command Line :C:\Freescale\KDS_v3\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.4.1.201603202153\win32\pegdbserver_console -device=NXP_KVx_KV30F64M10 -startserver -singlesession -serverport=7224 -interface=USBMULTILINK -speed=5000 -port=USB1 -configfil

 

 

 

 

CMD>RE

 

 

 

 

Initializing.

Target has been RESET and is active.

CMD>CM C:\Freescale\KDS_v3\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.4.1.201603202153\win32\gdi\P&E\supportFiles_ARM\NXP\KVx\freescale_kv30f64m10_1x32x16k_pflash.arp

 

 

 

 

Initializing.

Initialized.

 

 

 

 

;version 1.01, 02/23/2016, Copyright 2016 P&E Microcomputer Systems, Inc. All rights reserved. www.pemicro.com [kv_30f64_n_pflash]

 

 

 

 

;device freescale, kv30f64m10, 1x32x16k, desc=pflash

 

 

 

 

;begin_cs device=$00000000, length=$00010000, ram=$1FFFE000

 

 

 

 

Loading programming algorithm ...

Done.

CMD>EM

 

 

 

 

Erasing.

Module has been erased.

CMD>PM

 

 

 

 

Programming.

Processing Object File Data ...

                               

.

Programmed.

CMD>VC

Verifying object file CRC-16 to device ranges ...

   block 00000000-00003233 ...

Ok.

 

 

   Checksum Verification Successful. (Cumulative CRC-16=$DB07)

 

 

 

 

 

 

CMD>RE

 

 

 

 

Initializing.

Target has been RESET and is active.

 

 

 

 

WARNING - NO RESET SCRIPT FILE HAS BEEN CONFIGURED TO RUN!!!

 

 

TO MODIFY THE RESET SCRIPT SETTINGS, USE THE FOLLOWING MENU OPTION:

 

 

CONFIGURATION -> AUTOMATED SCRIPT OPTIONS

 

 

 

 

 

 

 

 

 

With regards;

Vaibhav

Original Attachment has been moved to: tbc_gpio.zip

Labels (1)
1 Solution
2,745 Views
DavidS
NXP Employee
NXP Employee

Hi Vaibhav,

I was able to run your project on my FRDM-K22F (I do not have FRDM-KV31) from debugger and from Power-On Reset.

You might add strong pull-up to PTC4 (NMI) signal.  It is enabled by default.

Or you can go into thte startup_MKV30F12810.S and modify the Flash Configuration field to disable NMI capability:

Default Flash Configuration:

    .section .FlashConfig, "a"

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFFFFFE

Modified Flash Configuration to disable NMI (FOPT[NMI]=0):

    .section .FlashConfig, "a"

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFFFBFE

Regards,

David

View solution in original post

8 Replies
2,745 Views
vaibhavsomani
Contributor II

DavidS
Hi can you see my code and suggest any solution ?

With regards;

Vaibhav Somani

0 Kudos
Reply
2,746 Views
DavidS
NXP Employee
NXP Employee

Hi Vaibhav,

I was able to run your project on my FRDM-K22F (I do not have FRDM-KV31) from debugger and from Power-On Reset.

You might add strong pull-up to PTC4 (NMI) signal.  It is enabled by default.

Or you can go into thte startup_MKV30F12810.S and modify the Flash Configuration field to disable NMI capability:

Default Flash Configuration:

    .section .FlashConfig, "a"

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFFFFFE

Modified Flash Configuration to disable NMI (FOPT[NMI]=0):

    .section .FlashConfig, "a"

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFFFFFF

    .long 0xFFFFFBFE

Regards,

David

2,746 Views
vaibhavsomani
Contributor II

Thanks DavidS once again !!

My problem is solved after changing code as suggested by you :smileyhappy:
and I found on my board NMI pin was pulled down. So i will make it pull-up.
You picked the problem very accurately :smileyhappy:

Thanks;
Vaibhav Somani

2,746 Views
DavidS
NXP Employee
NXP Employee

Glad to help and thank you for sharing your results.  It will help others too.

Regards,

David

0 Kudos
Reply
2,746 Views
vaibhavsomani
Contributor II

Thanks DavidSfor quick reply.
I have TWR-KV31F120M. My code is also working fine on TWR-KV31.
But when I am flashing same code on my board, on power on reset or reset through pin. It is not working.
In debug mode when jtag connector is connected, I tried to do reset via reset pin. My cursor/pointer is showing DefaultISR due to WDOG_EWM_IRQHandler() ??

And this is defined as dead loop in startup_MKV30F12810.S file. So whenever a reset or power on reset happens it is going to  DefaultISR and stuck in dead loop. Here is the screenshot ..

reset_pin_error.png

Please suggest how to overcome on this ?

0 Kudos
Reply
2,746 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Vaibhav Somani,

please, how do you have connected RESET pin?

Best Regards,

Iva

0 Kudos
Reply
2,746 Views
vaibhavsomani
Contributor II

Reset pin has a 100nF capacitor and pull up with 6.8k

resistor.

 

with regards;

Vaibhav

Somani

0 Kudos
Reply
2,746 Views
vaibhavsomani
Contributor II

Sorry for typo.
It is MKV30F64VLH10 .

0 Kudos
Reply