MKL28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKL28

2,717 Views
paolocolombo
Contributor III

Hi, I have to develop an application using MKL28.

MCUXpresso Config Tools support it and support Peripheral Configuration ?

Thanks.

Paolo Colombo

0 Kudos
Reply
3 Replies

2,522 Views
paolocolombo
Contributor III

Thanks for your reply.

The pins configuration is ok. But for the configuration of the peripheral? If I click on "Peripherals", I get this screen!

How can I configure timers or UARTS?

0 Kudos
Reply

2,522 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Paolo Colombo

Yes, MCUXpresso Config Tools support KL28 and support Peripheral Configuration.

pastedImage_1.png

Regards

Daniel


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,522 Views
paolocolombo
Contributor III

Thanks for your reply!

If I click on "Pins", I get your screen, but if I click on "Peripherals" I get a screen that says "MCU not supported".

How do I configure timers or UARTS or other peripheral?

Regards,

Paolo

0 Kudos
Reply