MK60DN512VLQ10 UART questions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK60DN512VLQ10 UART questions

844 Views
henrynguyen
Contributor IV

Hello,

 

I would like to configure two uarts using processor expert: UART 0 for display text message to the hyper terminal and UART 1 for communication to another board (non NXP chip) for a 3 Mbps uart comm w/o flow control.  I am not using TWR tower.  Our existing project already have two comm boards using uart at 3 Mbps w/o flow control.  we are trying to upgrade the processor.

 

I added the uartCom component from KSDK 1.3 and then start configuring my baudrate, call back function, etc.

Hit generate, i can see the codes in project/SDK/platform/drivers/src/fsl_uart_driver.c and so on.

however, upon opening them, i see that all key functions like init, send, receive, etc are commented out. 

it is because of the #if FSL_FEATURE_SOC_UART_COUNT which is not defined.

 

can you please advise on what i am missing here?

 

attached pix shows my project, top part of fsl_uart_driver.c which codes got grayed out and my PE UART configuration.

 

Thank you for your help.

Henry

Labels (1)
0 Kudos
Reply
0 Replies