MK20DX256VLL7 Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK20DX256VLL7 Support

1,422件の閲覧回数
mayanksirotiya
Contributor I

Hello, I am trying to build KSDK for MK20DX256VLL7 processor. But i couldn't find it in the list, the closest I could see is MK20DX256VLL10, which has a different Maximum CPU Frequency as 10 instead of 7. Is it safe to use KSDK build with MK20DX256VLL10 for MK20DX256VLL7? I am asking this as I facing some problems with flashing the binary onto MK20DX256VLL7 processor built with KSDK MK20DX256VLL10.

ラベル(1)
0 件の賞賛
返信
1 返信

1,309件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Mayank.

I  apologize for my late response.

It is not just about different speed and they are different dies.

There isn’t any test executed internally for the xxx7 parts.

The SDK driver should be compatible for all chips because SDK driver is designed as a common code base for all SoCs with same IP integrated. However, we don’t provide the feature file for these XXX7 parts thus the SDK driver can’t work for these parts. 

Best Regards,

Iva

0 件の賞賛
返信