MK20DX256VLL7 Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK20DX256VLL7 Support

1,381 Views
mayanksirotiya
Contributor I

Hello, I am trying to build KSDK for MK20DX256VLL7 processor. But i couldn't find it in the list, the closest I could see is MK20DX256VLL10, which has a different Maximum CPU Frequency as 10 instead of 7. Is it safe to use KSDK build with MK20DX256VLL10 for MK20DX256VLL7? I am asking this as I facing some problems with flashing the binary onto MK20DX256VLL7 processor built with KSDK MK20DX256VLL10.

Labels (1)
0 Kudos
Reply
1 Reply

1,268 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Mayank.

I  apologize for my late response.

It is not just about different speed and they are different dies.

There isn’t any test executed internally for the xxx7 parts.

The SDK driver should be compatible for all chips because SDK driver is designed as a common code base for all SoCs with same IP integrated. However, we don’t provide the feature file for these XXX7 parts thus the SDK driver can’t work for these parts. 

Best Regards,

Iva

0 Kudos
Reply