MK20DX256VLL10 SPI Driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MK20DX256VLL10 SPI Driver

1,695 次查看
pmasanek1
Contributor I

I am using MCUExpresso IDE v11.0.0. My project us using MK20DX256VLL10 and I need SPI1 to operate a Touch LCD screen. I have assigned Pins for this, and with the Pins screen the SPI Peripheral shows with a check and green box. However, going to the Peripheral screen, SPI is not present. The IDE does not show a driver missing (FSL_SPI?). How do I complete adding SPI to this project?

0 项奖励
回复
1 回复

1,597 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Paul,

 

You can get the drivers from the corresponding SDK. Please check the link below to download the SDK.

Welcome | MCUXpresso SDK Builder 

I hope it helps!

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复