MK10DX256VLH7 Support in KSDK 2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MK10DX256VLH7 Support in KSDK 2.0

955 Views
santosh1
Contributor III

Hello, 

The SDK builder hosted at kex.nxp.com doesn't seem to be supporting MK10DX256VLH7. Uploading a new configuration with processor changed also does not help. Is there any way to download the full SDK or is this controller not supported at all?

Labels (1)
0 Kudos
Reply
2 Replies

821 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Santosh,

Unfortunately there is no KSDK support for MK10DX256VLH7.

Anyway, you can start your program with PEx and KDS.

MK10.png

Or you can start with www.nxp.com/mqx also see the support for TWR-K20D72M

For MQX 4.2 is under

C:\Freescale\Freescale_MQX_4_2\mqx\examples

I hope this helps.

Best Regards,

Iva

0 Kudos
Reply

821 Views
santosh1
Contributor III

Iva, 

Thanks for the quick response. I already have a project in KSDK 2.0 with MK22 and i was hoping to reuse a significant chunk that interfaces with a module for the MK10DX256VLH7 based project. i was hoping to create a project with MK10DX256XXX10 as the base with KSDK2.0 and just use that. Will that not work?  

Thanks

0 Kudos
Reply