I am using tower board TWRK60D100M with 700-27291 REVA board.When I checked the data sheet,the one which is existing is not matching with the case of jumper for example J19 jumper information is not present in the data sheet.I am trying to give the target power through Jtag after enabling the target voltage from Jtag side by giving Power on perm through Jtag commander tool.But it not detecting 5 volt on the target side which I doubt of not placing the corresponding jumper on the board.#twr-k60d100m