LCD Implementation in FRDM K64F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD Implementation in FRDM K64F

ソリューションへジャンプ
5,684件の閲覧回数
rahul_eris
Fresh Out Contributor

Hi,

 

I am using frdm k64f board and KDS IDE for my project.

I need to implement LCD on it.  Either in 8 bit or 4 bit mode.

 

I cannot see any driver for lcd in KDS or KSDK.

So i wrote my own driver for lcd.

But its not working .( Displayed the string 2,3 times but not consistent, as its not displaying always after reprogramming )

 

LCD Driver code is shown below.............................

 

 

void delay( int msec)

{

  int i,j;

  for(i=0;i<msec;i++)

       for(j=0; j<1270; j++);

}

 

 

void lcd_cmd( char DData) // Function to send command on LCD

{

  GPIO_DRV_WritePinOutput(kGpioLCDEN, 0);

 

  if((DData & 0x01) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD0, 0);

  else

  {

  GPIO_DRV_WritePinOutput(kGpioLCDD0, 1);

  }

  if((DData & 0x02) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD1, 0);

  else

  {

  GPIO_DRV_WritePinOutput(kGpioLCDD1, 1);

  }

  if((DData & 0x04) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD2, 0);

  else

  {

  GPIO_DRV_WritePinOutput(kGpioLCDD2, 1);

  }

  if((DData & 0x08) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD3, 0);

  else

  {

  GPIO_DRV_WritePinOutput(kGpioLCDD3, 1);

  }

  if((DData & 0x10) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD4, 0);

  else

  {

  GPIO_DRV_WritePinOutput(kGpioLCDD4, 1);

  }

  if((DData & 0x20) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD5, 0);

  else

  {

  GPIO_DRV_WritePinOutput(kGpioLCDD5, 1);

  }

  if((DData & 0x40) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD6, 0);

  else

  {

  GPIO_DRV_WritePinOutput(kGpioLCDD6, 1);

  }

  if((DData & 0x80) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD7, 0);

  else

  {

  GPIO_DRV_WritePinOutput(kGpioLCDD7, 1);

  }

 

  GPIO_DRV_WritePinOutput(kGpioLCDRS, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDRW, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDEN, 1);

  delay(8);

  GPIO_DRV_WritePinOutput(kGpioLCDEN, 0);

  delay(1);

}

 

 

 

 

void lcd_data(char DData) // Function to display character on LCD

{

  GPIO_DRV_WritePinOutput(kGpioLCDEN, 0);

 

if((DData & 0x01) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD0, 0);

  else

  GPIO_DRV_WritePinOutput(kGpioLCDD0, 1);

 

  if((DData & 0x02) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD1, 0);

  else

  GPIO_DRV_WritePinOutput(kGpioLCDD1, 1);

 

  if((DData & 0x04) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD2, 0);

  else

  GPIO_DRV_WritePinOutput(kGpioLCDD2, 1);

 

  if((DData & 0x08) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD3, 0);

  else

  GPIO_DRV_WritePinOutput(kGpioLCDD3, 1);

 

  if((DData & 0x10) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD4, 0);

  else

  GPIO_DRV_WritePinOutput(kGpioLCDD4, 1);

 

  if((DData & 0x20) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD5, 0);

  else

  GPIO_DRV_WritePinOutput(kGpioLCDD5, 1);

 

  if((DData & 0x40) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD6, 0);

  else

  GPIO_DRV_WritePinOutput(kGpioLCDD6, 1);

 

  if((DData & 0x80) ==0)

  GPIO_DRV_WritePinOutput(kGpioLCDD7, 0);

  else

  GPIO_DRV_WritePinOutput(kGpioLCDD7, 1);

 

  GPIO_DRV_WritePinOutput(kGpioLCDRS, 1);

  GPIO_DRV_WritePinOutput(kGpioLCDRW, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDEN, 1);

  delay(8);

  GPIO_DRV_WritePinOutput(kGpioLCDEN, 0);

  delay(1);

}

 

 

void lcd_data_string( char *lcd_str)

{

  int i=0;

  while(lcd_str[i]!='\0')

  {

  lcd_data(lcd_str[i]);

  i++;

  delay(1);

  }

}

 

 

void goto_xy(int x,int y)

{

   if(x==0||x==1)

    lcd_cmd(0X80+y);

   if(x==2)

    lcd_cmd(0XC0+y);

  }

 

 

void init_lcd()

{

  GPIO_DRV_WritePinOutput(kGpioLCDRS, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDRW, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDEN, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDD0, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDD1, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDD2, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDD3, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDD4, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDD5, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDD6, 0);

  GPIO_DRV_WritePinOutput(kGpioLCDD7, 0);

 

  lcd_cmd(0X38);   // For using 8-bit 2 row LCD

  delay(1);

  lcd_cmd(0X01); // For clear LCD screen

  delay(1);

  lcd_cmd(0X0C); // For display on cursor off

  delay(1);

  lcd_cmd(0X80);

  delay(10);

 

  lcd_data_string("CHECK LCD");

}

 

.............................

 

All pins are configured as output pin and connected  successfully.

 

I cant findout the mistake in this as all commands and datas given through the above code is getting to the lcd pins.(Verified through multimeter)

Replaced the lcd module  and the problem still exists.

 

How this problem could be solved?? ?? I am blocked with this and delayed in our development activity.

Hoping for a solution asap.

 

 

 

 

 

 

Thanks,

Rahul

 

TRIVANDRUM

ラベル(1)
タグ(2)
1 解決策
4,377件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Rahul,

I am glad to know your application works properly, anyway I would like to recommend the following document:

Driving 16x2 LCD using KSDK drivers

The application uses the FRDM-KL25, but I assume you can use the same principle in your application.

I hope this material will be useful for you.

Have a great day.

David

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,377件の閲覧回数
joseagustinbarr
Contributor I

Could you post the entire project? I am trying to get an example of a 16x2 lcd display with no success. Thank you.

0 件の賞賛
返信
4,377件の閲覧回数
rahul_eris
Fresh Out Contributor

Hello All,

The code worked . Issue were in the delay call.

I have used _time_delay() instead of the one used earlier.

Thank you.

Rahul

0 件の賞賛
返信
4,378件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Rahul,

I am glad to know your application works properly, anyway I would like to recommend the following document:

Driving 16x2 LCD using KSDK drivers

The application uses the FRDM-KL25, but I assume you can use the same principle in your application.

I hope this material will be useful for you.

Have a great day.

David

0 件の賞賛
返信
4,377件の閲覧回数
rahul_eris
Fresh Out Contributor

Hello David,

Thanks  for the document.This is a needed document for LCD driver implementation .

Thanks

Rahul

0 件の賞賛
返信