KinetisFlashTool download program speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KinetisFlashTool download program speed

1,418 Views
hansonhe
NXP Employee
NXP Employee

Dear,

Customer name: Tianyu

Project: mPos

PartNumber: KL81Z128VMC7

We use KinetisFlashTool from NXP_Kinetis_Bootloader_2_0_0\bin\Tools\KinetisFlashTool\win

 for MP tools downloading, but find it is slowly, when download about 70K program, it will need about 20s by USB port.

We need speed up to about 5s for one equipement production, do you have some method to do the performance optimization for this GUI tools. Thanks.

0 Kudos
Reply
1 Reply

1,227 Views
hansonhe
NXP Employee
NXP Employee

Dear,

Do you have some update? Customer use it for mass production tools, we need improve the efficiency of the tools. 

0 Kudos
Reply