Kinetis bootloader and KSDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis bootloader and KSDK

1,827 Views
kalden_srcinc
Contributor IV

Are there any plans to update the Kinetis bootloader to be more integrated with the KSDK?  It appears to provide its own set of drivers and boot code right now.  Also, is Ethernet support planned?

 

Thanks

Labels (1)
1 Reply

1,572 Views
mjbcswitzerland
Specialist V

Kevin

If you are in need of KBOOT compatibility and Ethernet support you can also look at

http://www.utasker.com/kinetis.html

where loaders are available for almost all Freescale boards/parts - including Ethernet.
Unlike the KBOOT original sources they can be built with almost any IDE.

I have heard that the next KBOOT version is planned for June 2015 and that USB-MSD may be included (although which parts will be supported is not known - the last release from December 2014 actually reduced the supported parts for some reason).

The uTasker loader can be used with any application (it is often used with MQX applications) but its code actually is shared with the uTasker application framework (that is, all drivers, generic protocols, OS are the same source).

It will be interesting to see whether the next KBOOT release will bring together its sources, but I don't expect this will be the case since they are probably developed by different groups who look to have started with different code bases.

Regards

Mark

0 Kudos
Reply