Kinetis SDK Support for K60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis SDK Support for K60

ソリューションへジャンプ
1,960件の閲覧回数
w2vy
Contributor V

I am reviving an old CodeWarrior w/MQX project and decided it would be a good idea to give KDS a try.

 

So I installed KDS and KSDK and found that my variant was not supported yet.

 

I see K63F/K64F support, is there any support expected for the older variants?

Is it possible to manually create the files needed to add specific support?

 

Tom

ラベル(1)
1 解決策
1,763件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

The KSDK support for the legacy Kinetis devices is planned and will come with the next KSDK  releases. The KSDK v1.1 release is planned for this month and it will include support for some older devices.


Hope this information can help you.

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,764件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

The KSDK support for the legacy Kinetis devices is planned and will come with the next KSDK  releases. The KSDK v1.1 release is planned for this month and it will include support for some older devices.


Hope this information can help you.

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------