Kinetis SDK Project Generator v2 - Windows 10 Support?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis SDK Project Generator v2 - Windows 10 Support?

1,593件の閲覧回数
Deejay
Contributor III

Hi,

I wonder if this is supported on Windows10 platform as I get the following error message:

"This app can't run on your PC. To find a version for your PC, check with the software publisher."

Any idea or work-around solution to run on Windows 10??

Thanks.

 

Regards,

DJ

ラベル(1)
0 件の賞賛
返信
1 返信

1,482件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

officially KSDK generator v2 doesn't support win10.

This product has been tested on the following system configurations:

pastedImage_1.png

this information is documented in KSDK Project Generator Release Notes - 2.1.pdf under Kinetis SDK Project Generator v2 folder.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信