Kinetis 3.0.0 and KSDK_1.2.0 won't install on Windows 7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis 3.0.0 and KSDK_1.2.0 won't install on Windows 7

869 Views
rnk2014
Contributor II

I'm trying to update to Kinetis 3.0.0 based on the most recent releases on Linux (Fedora 21).

 

Once I've installed the design studio, and then installed the SDK, I need to "install software" under eclipse.  This is done by installing a zipfile contained in the SDK.

 

The process begins okay but halfway through the installation it claims that certain GTK files are missing.

 

Is anyone else struggling with this?

 

My goal is to at least successfully write a couple test programs for the KL25Z, but up til now, I've only been successful with MBED.

 

Rich

Labels (1)
0 Kudos
Reply
1 Reply

765 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Rich,

Please, are you trying update KDS 3.0 and KSDK 1.2 on Windows or Linux? In header you mentioned Windows.

Do you have 64-bit installation package for Linux? KDS 2.0 and KSDK 1.1 does work on Fedora without problems?

Did you follow all instructions for installation RPM?

Please, what GTK files are missing? Please, can you make a screenshot of the error/warning message? Is it error or warning - after this message, is installation completed?

Are you able to flash any demo to your board?

Thank you for your feedback.

Best Regards,

Iva

0 Kudos
Reply