KSKD 1.3 / TWR-K65 / Ethernet Serial Demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSKD 1.3 / TWR-K65 / Ethernet Serial Demo

1,688 Views
HeMyFAE
NXP Employee
NXP Employee

KSKD 1.3 / TWR-K65 / Ethernet Serial Demo

 

Dear KsDK 1.3 support team,

 

I am having a bit of problem recompiling the Ethernet to Serial DEmo program for KSKD1.3 / TWR-K65.

The demo prgram is under this folder:

C:\Freescale\KSDK_1.3.0\middleware\tcpip\rtcs\examples\eth_to_serial\build\kds\eth_to_serial_twrk65f180m

As you can see, from my attached screen capture, I have recompiled the lib, platform, rtsc projects.

There is fatal error "There is no such file or directory for Psptypes.h"

include "psptypes.h"

 

I located where that file an and added to the link resources path for it but it still won't compiled.

Please advise!

Thx,

hy

Labels (1)
0 Kudos
Reply
1 Reply

1,530 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mai,

When you want run one MQX demo , and you do not clearly which lib need to be build ,

i recommend you import the project use "MQX->Import Working Sets":

pastedImage_0.png

pastedImage_1.png

then "build all"

pastedImage_2.png

You can see there is no error :

pastedImage_3.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply