KSDK2.0 definition kUART_RxFifoOverflowInterruptEnable in fsl_uart.h

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSDK2.0 definition kUART_RxFifoOverflowInterruptEnable in fsl_uart.h

1,109件の閲覧回数
manfredschnell
Contributor IV

Hello,

 

in KSDK2.0 file "fsl_uart.h" line 106 I think there is a typo error:

    kUART_RxFifoOverflowInterruptEnable = (UART_CFIFO_TXOFE_MASK << 24),  /*!< TX FIFO overflow interrupt. */

    kUART_TxFifoOverflowInterruptEnable = (UART_CFIFO_RXUFE_MASK << 24),  /*!< RX FIFO underflow interrupt. */

    kUART_RxFifoUnderflowInterruptEnable = (UART_CFIFO_RXUFE_MASK << 24), /*!< RX FIFO underflow interrupt. /

 

I think it should be:

    kUART_RxFifoOverflowInterruptEnable = (UART_CFIFO_RXOFE_MASK << 24),  /*!< TX FIFO overflow interrupt. */

    kUART_TxFifoOverflowInterruptEnable = (UART_CFIFO_TXOFE_MASK << 24),  /*!< RX FIFO underflow interrupt. */

    kUART_RxFifoUnderflowInterruptEnable = (UART_CFIFO_RXUFE_MASK << 24), /*!< RX FIFO underflow interrupt.*/

 

Best regards

Manfred

ラベル(1)
0 件の賞賛
返信
1 返信

963件の閲覧回数
Jmart
NXP Employee
NXP Employee

Manfred,

Thanks for the feedback. I've asked the team to look into this.

Thanks,

Jason

0 件の賞賛
返信