KSDK2.0 EDMA_HandleIRQ callback calls NULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KSDK2.0 EDMA_HandleIRQ callback calls NULL

Jump to solution
1,651 Views
manfredschnell
Contributor IV

Hello,

 

we use KSDK2.0 with K64.

 

In Function EDMA_HandleIRQ() "fsl_edma.c" the handle->callback() is called regardless if it's NULL. --> This leads to HardFault.

 

The "Kinetis SDK v.2.0 API Reference Manual.pdf" on page 221 writes relating to that:

 

 

 

 

 

"16.7.38  void EDMA_HandleIRQ (edma_handle_t *  handle )

 

 

 

 

This function clears the channel major interrupt flag and call the callback function if it is not NULL."

 

 

Next KSDK source should be changed to call the callback only, if it's not NULL.

 

Best regards

Manfred

 

 


 

Labels (1)
1 Solution
1,441 Views
Jmart
NXP Employee
NXP Employee

Manfred,

I've confirmed that this code is updated already and will be available in the next release of the edma driver enabled parts.

if ((handle->tcdPool == NULL) && (handle->callback != NULL))

    {

        (handle->callback)(handle, handle->userData, true, 0);

    }

/* Invoke callback function. */

        if (handle->callback)

        {

            (handle->callback)(handle, handle->userData, transfer_done, tcds_done);

        }

Thanks for your feedback,

Jason

View solution in original post

0 Kudos
Reply
1 Reply
1,442 Views
Jmart
NXP Employee
NXP Employee

Manfred,

I've confirmed that this code is updated already and will be available in the next release of the edma driver enabled parts.

if ((handle->tcdPool == NULL) && (handle->callback != NULL))

    {

        (handle->callback)(handle, handle->userData, true, 0);

    }

/* Invoke callback function. */

        if (handle->callback)

        {

            (handle->callback)(handle, handle->userData, transfer_done, tcds_done);

        }

Thanks for your feedback,

Jason

0 Kudos
Reply