KSDK v2.0 - Peripheral registers access

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSDK v2.0 - Peripheral registers access

4,073件の閲覧回数
shauldorf
Contributor V

How peripheral registers (PORT, GPIO, I2C, FTM) can be directly accessed (modified) using “C” or “C++” ?

For example Using K64 in KSDK 1.3 all registers are defined in “MK64F12.h”. Using KSDK 2,0 in the same named file peripheral registers definition is missing.

ラベル(1)
タグ(1)
0 件の賞賛
返信
8 返答(返信)

3,406件の閲覧回数
shauldorf
Contributor V

Thanks

 

Yes I already have done it myself.

Using KSDK v2.0 I have two working Edge aligned PWMs projects,

One without API only registers configuration and the other using FTM API.

 

BR

Shaul  :smileywink::smileycheck:

 

 

3,406件の閲覧回数
shauldorf
Contributor V

My problem is with Channel(n) Status And Control (FTM0_C0SC, FTM1_C0SC … ),

How to define array of n.

 

I’m not familiar with those definition in MK64F12.h

 

 

struct {                                         /* offset: 0xC, array step: 0x8 */

   __IO uint32_t CnSC;                             /**< Channel (n) Status And Control, array offset: 0xC, array step: 0x8 */

   __IO uint32_t CnV;                               /**< Channel (n) Value, array offset: 0x10, array step: 0x8 */

How to define CnSC and CnV  ??

Shaul

 

 

0 件の賞賛
返信

3,406件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Shaul,

How about using the code:

access FTM0 register:

FTM0->CONTROLS[0].CnSC=0x0000;  //access the FTM0_C0SC

FTM0->CONTROLS[1].CnSC=0x0000;  //access the FTM0_C1SC

FTM0->CONTROLS[0].CnV=0x0000;  //access the FTM0_C0V

FTM0->CONTROLS[1].CnV=0x0000;  //access the FTM0_C1V

access FTM1 register:

FTM1->CONTROLS[0].CnSC=0x0000;  //access the FTM1_C0SC

FTM1->CONTROLS[1].CnSC=0x0000;  //access the FTM1_C1SC

FTM1->CONTROLS[0].CnV=0x0000;  //access the FTM1_C0V

FTM1->CONTROLS[1].CnV=0x0000;  //access the FTM1_C1V

Hope it can help you

BR

Xiangjun Rong

0 件の賞賛
返信

3,406件の閲覧回数
shauldorf
Contributor V

Thanks again

Yes I’m interested in KSDK 2.0

I’m considering to change to KSDK 2.0 and I want to compare and understand the meaning of direct register access without API.

My intention is to convert this simple example from KSDK1.3 to KSDK 2.0

 

#include "MK64F12.h"

static int i = 0;

 int main(void)

{

       SIM_SCGC5 |= 0x800;

       PORTC_PCR4 = 0x400;

       PORTC_PCR1 = 0x400;

       PORTC_PCR2 = 0x400;

       PORTC_PCR3 = 0x400;

 

       SIM_SCGC6|=0x03000000;

       FTM0_CONF=0xC0;

       FTM0_FMS=0x00;

       FTM0_MODE|=0x05;

       FTM0_MOD=1000;

       FTM0_C0SC=0x28;

       FTM0_C1SC=0x28;

       FTM0_COMBINE=0x02;

       FTM0_COMBINE|=0x10;

BR

Shaul

0 件の賞賛
返信

3,406件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

you can use the code to access FTM0 register based on SDK2.0 and KDS tools:

FTM0->CONF=0xxx; //FTM0_CONF=0xC0;

FTM0->FMS=0x0000; //FTM0_FMS=0x00;

for PORTC register access:

PORTC->PCR[4]=0xxx;  //PORTC_PCR4 = 0x400;

For SIM module

SIM->SCGC6|=0x03000000;

Hope it can help you.

BR

Xiangjun Rong

typedef struct {
  __IO uint32_t SC;                                /**< Status And Control, offset: 0x0 */
  __IO uint32_t CNT;                               /**< Counter, offset: 0x4 */
  __IO uint32_t MOD;                               /**< Modulo, offset: 0x8 */
  struct {                                         /* offset: 0xC, array step: 0x8 */
    __IO uint32_t CnSC;                              /**< Channel (n) Status And Control, array offset: 0xC, array step: 0x8 */
    __IO uint32_t CnV;                               /**< Channel (n) Value, array offset: 0x10, array step: 0x8 */
  } CONTROLS[8];
  __IO uint32_t CNTIN;                             /**< Counter Initial Value, offset: 0x4C */
  __IO uint32_t STATUS;                            /**< Capture And Compare Status, offset: 0x50 */
  __IO uint32_t MODE;                              /**< Features Mode Selection, offset: 0x54 */
  __IO uint32_t SYNC;                              /**< Synchronization, offset: 0x58 */
  __IO uint32_t OUTINIT;                           /**< Initial State For Channels Output, offset: 0x5C */
  __IO uint32_t OUTMASK;                           /**< Output Mask, offset: 0x60 */
  __IO uint32_t COMBINE;                           /**< Function For Linked Channels, offset: 0x64 */
  __IO uint32_t DEADTIME;                          /**< Deadtime Insertion Control, offset: 0x68 */
  __IO uint32_t EXTTRIG;                           /**< FTM External Trigger, offset: 0x6C */
  __IO uint32_t POL;                               /**< Channels Polarity, offset: 0x70 */
  __IO uint32_t FMS;                               /**< Fault Mode Status, offset: 0x74 */
  __IO uint32_t FILTER;                            /**< Input Capture Filter Control, offset: 0x78 */
  __IO uint32_t FLTCTRL;                           /**< Fault Control, offset: 0x7C */
  __IO uint32_t QDCTRL;                            /**< Quadrature Decoder Control And Status, offset: 0x80 */
  __IO uint32_t CONF;                              /**< Configuration, offset: 0x84 */
  __IO uint32_t FLTPOL;                            /**< FTM Fault Input Polarity, offset: 0x88 */
  __IO uint32_t SYNCONF;                           /**< Synchronization Configuration, offset: 0x8C */
  __IO uint32_t INVCTRL;                           /**< FTM Inverting Control, offset: 0x90 */
  __IO uint32_t SWOCTRL;                           /**< FTM Software Output Control, offset: 0x94 */
  __IO uint32_t PWMLOAD;                           /**< FTM PWM Load, offset: 0x98 */
} FTM_Type;

0 件の賞賛
返信

3,406件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I just give an example for PORT B.

This is a structure defined in MK64F12.h

typedef struct {
  __IO uint32_t PCR[32];                           /**< Pin Control Register n, array offset: 0x0, array step: 0x4 */
  __O  uint32_t GPCLR;                             /**< Global Pin Control Low Register, offset: 0x80 */
  __O  uint32_t GPCHR;                             /**< Global Pin Control High Register, offset: 0x84 */
       uint8_t RESERVED_0[24];
  __IO uint32_t ISFR;                              /**< Interrupt Status Flag Register, offset: 0xA0 */
       uint8_t RESERVED_1[28];
  __IO uint32_t DFER;                              /**< Digital Filter Enable Register, offset: 0xC0 */
  __IO uint32_t DFCR;                              /**< Digital Filter Clock Register, offset: 0xC4 */
  __IO uint32_t DFWR;                              /**< Digital Filter Width Register, offset: 0xC8 */
} PORT_Type;

/** Peripheral PORTB base address */
#define PORTB_BASE                               (0x4004A000u)
/** Peripheral PORTB base pointer */
#define PORTB                                    ((PORT_Type *)PORTB_BASE)

For example, this is a  GPIO structure.

typedef struct {
  __IO uint32_t PDOR;                              /**< Port Data Output Register, offset: 0x0 */
  __O  uint32_t PSOR;                              /**< Port Set Output Register, offset: 0x4 */
  __O  uint32_t PCOR;                              /**< Port Clear Output Register, offset: 0x8 */
  __O  uint32_t PTOR;                              /**< Port Toggle Output Register, offset: 0xC */
  __I  uint32_t PDIR;                              /**< Port Data Input Register, offset: 0x10 */
  __IO uint32_t PDDR;                              /**< Port Data Direction Register, offset: 0x14 */
} GPIO_Type;

/** Peripheral PTB base address */
#define PTB_BASE                                 (0x400FF040u)
/** Peripheral PTB base pointer */
#define PTB                                      ((GPIO_Type *)PTB_BASE)

#define GPIOB                                    PTB

PORTB->PCR[0]=0x00;  //code written by Rong

GPIOB->PTOR|=0x0001; //code written by Rong

Hope it can help you.

BR

Xiangjun Rong

0 件の賞賛
返信

3,406件の閲覧回数
shauldorf
Contributor V

RONG Thanks

I’m hardware oriented and KSDK 1.3 version is very clear option.

Yours GPIO and PORTB example is clear.

I have difficulty id understanding FTMx_CnV (x and n options)

I would appreciate if you will provide few FTM code samples like:

FTM0_CONF

FTM0_CONF

FTM0_C0SC

FTM0_C1SC

FTM0_C1V

FTM0_C2SC

FTM0_COMBINE

BR

Shaul

0 件の賞賛
返信

3,406件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I am sorry, I had thought you used SDK2.0, as you know that SDK2.0 is different from SDK1.3. If you use SDK1.3, the SDK1.3 defines a lot of Hal function, you'd better use the hal function directly. For FTM module, pls refer to fsl_ftm_hal.h for the FTM hal function.

Regarding your question how to access register for FTM. Pls refer to MK60D10.h, I copy it here, you can see how to access FTM register based on SDK1.3.

BR

Xiangjun Rong

/** FTM - Register Layout Typedef */
typedef struct {
  __IO uint32_t SC;                                /**< Status And Control, offset: 0x0 */
  __IO uint32_t CNT;                               /**< Counter, offset: 0x4 */
  __IO uint32_t MOD;                               /**< Modulo, offset: 0x8 */
  struct {                                         /* offset: 0xC, array step: 0x8 */
    __IO uint32_t CnSC;                              /**< Channel (n) Status And Control, array offset: 0xC, array step: 0x8 */
    __IO uint32_t CnV;                               /**< Channel (n) Value, array offset: 0x10, array step: 0x8 */
  } CONTROLS[8];
  __IO uint32_t CNTIN;                             /**< Counter Initial Value, offset: 0x4C */
  __IO uint32_t STATUS;                            /**< Capture And Compare Status, offset: 0x50 */
  __IO uint32_t MODE;                              /**< Features Mode Selection, offset: 0x54 */
  __IO uint32_t SYNC;                              /**< Synchronization, offset: 0x58 */
  __IO uint32_t OUTINIT;                           /**< Initial State For Channels Output, offset: 0x5C */
  __IO uint32_t OUTMASK;                           /**< Output Mask, offset: 0x60 */
  __IO uint32_t COMBINE;                           /**< Function For Linked Channels, offset: 0x64 */
  __IO uint32_t DEADTIME;                          /**< Deadtime Insertion Control, offset: 0x68 */
  __IO uint32_t EXTTRIG;                           /**< FTM External Trigger, offset: 0x6C */
  __IO uint32_t POL;                               /**< Channels Polarity, offset: 0x70 */
  __IO uint32_t FMS;                               /**< Fault Mode Status, offset: 0x74 */
  __IO uint32_t FILTER;                            /**< Input Capture Filter Control, offset: 0x78 */
  __IO uint32_t FLTCTRL;                           /**< Fault Control, offset: 0x7C */
  __IO uint32_t QDCTRL;                            /**< Quadrature Decoder Control And Status, offset: 0x80 */
  __IO uint32_t CONF;                              /**< Configuration, offset: 0x84 */
  __IO uint32_t FLTPOL;                            /**< FTM Fault Input Polarity, offset: 0x88 */
  __IO uint32_t SYNCONF;                           /**< Synchronization Configuration, offset: 0x8C */
  __IO uint32_t INVCTRL;                           /**< FTM Inverting Control, offset: 0x90 */
  __IO uint32_t SWOCTRL;                           /**< FTM Software Output Control, offset: 0x94 */
  __IO uint32_t PWMLOAD;                           /**< FTM PWM Load, offset: 0x98 */
} FTM_Type, *FTM_MemMapPtr;

/* ----------------------------------------------------------------------------
   -- FTM - Register accessor macros
   ---------------------------------------------------------------------------- */

/*!
 * @addtogroup FTM_Register_Accessor_Macros FTM - Register accessor macros
 * @{
 */


/* FTM - Register accessors */
#define FTM_SC_REG(base)                         ((base)->SC)
#define FTM_CNT_REG(base)                        ((base)->CNT)
#define FTM_MOD_REG(base)                        ((base)->MOD)
#define FTM_CnSC_REG(base,index)                 ((base)->CONTROLS[index].CnSC)
#define FTM_CnSC_COUNT                           8
#define FTM_CnV_REG(base,index)                  ((base)->CONTROLS[index].CnV)
#define FTM_CnV_COUNT                            8
#define FTM_CNTIN_REG(base)                      ((base)->CNTIN)
#define FTM_STATUS_REG(base)                     ((base)->STATUS)
#define FTM_MODE_REG(base)                       ((base)->MODE)
#define FTM_SYNC_REG(base)                       ((base)->SYNC)
#define FTM_OUTINIT_REG(base)                    ((base)->OUTINIT)
#define FTM_OUTMASK_REG(base)                    ((base)->OUTMASK)
#define FTM_COMBINE_REG(base)                    ((base)->COMBINE)
#define FTM_DEADTIME_REG(base)                   ((base)->DEADTIME)
#define FTM_EXTTRIG_REG(base)                    ((base)->EXTTRIG)
#define FTM_POL_REG(base)                        ((base)->POL)
#define FTM_FMS_REG(base)                        ((base)->FMS)
#define FTM_FILTER_REG(base)                     ((base)->FILTER)
#define FTM_FLTCTRL_REG(base)                    ((base)->FLTCTRL)
#define FTM_QDCTRL_REG(base)                     ((base)->QDCTRL)
#define FTM_CONF_REG(base)                       ((base)->CONF)
#define FTM_FLTPOL_REG(base)                     ((base)->FLTPOL)
#define FTM_SYNCONF_REG(base)                    ((base)->SYNCONF)
#define FTM_INVCTRL_REG(base)                    ((base)->INVCTRL)
#define FTM_SWOCTRL_REG(base)                    ((base)->SWOCTRL)
#define FTM_PWMLOAD_REG(base)                    ((base)->PWMLOAD)

/** Peripheral FTM0 base address */
#define FTM0_BASE                                (0x40038000u)
/** Peripheral FTM0 base pointer */
#define FTM0                                     ((FTM_Type *)FTM0_BASE)

#define FTM0_CnV(index)                          FTM_CnV_REG(FTM0,index)

If you want to access the FTM0_C1V register, you can use the code

uint16_t temp;

temp=FTM0_CnV(1) ;

0 件の賞賛
返信