I am just starting with the FRDM_K22F board and need the ADC in 16bit resolution which I though was supported by this CPU.
However looking through the SDK API documentation, there only appear to be resolution settings for up to 13 bits in the enum adc_resultion_mode_t.
Am I looking in the wrong place or is 16bit not supported in the SDK?
The documentation does not show it but it turns out that in the fsl_adc_hal.h there are a couple of extra lines in the adc_resolution_mode_t enum:
#if (FSL_FEATURE_ADC_MAX_RESOLUTION>=16)
, kAdcResolutionBitOf16 = 3U,
/*!< 16-bit for both single end sample and differential sample. */
kAdcResolutionBitOfSingleEndAs16 = kAdcResolutionBitOf16, /*!< 16-bit for single end sample. */
kAdcResolutionBitOfDiffModeAs16 = kAdcResolutionBitOf16 /*!< 16-bit for differential sample. */
#endif /* FSL_FEATURE_ADC_MAX_RESOLUTION */
Hi Marco,
When customer want to modify resolutionMode value, it need to modify at [ksdk_platform_lib] project <fsl_adc_driver.c> below function:
/*FUNCTION*********************************************************************
*
* Function Name : ADC_DRV_StructInitUserConfigForIntMode
* Description : Fill the initial user configuration for interrupt mode.
* Then call initialization function with the filled parameter would configure
* the ADC module work as the interrupt mode.
*
*END*************************************************************************/
adc_status_t ADC_DRV_StructInitUserConfigForIntMode(adc_user_config_t *userConfigPtr)
{
if ( !userConfigPtr )
{
return kStatus_ADC_InvalidArgument;
}
userConfigPtr->intEnable = true;
userConfigPtr->lowPowerEnable = true;
userConfigPtr->clkDividerMode = kAdcClkDividerInputOf8;
userConfigPtr->resolutionMode = kAdcResolutionBitOf12or13;
userConfigPtr->clkSrcMode = kAdcClkSrcOfAsynClk;
userConfigPtr->asyncClkEnable = true;
userConfigPtr->highSpeedEnable = false;
userConfigPtr->hwTriggerEnable = false;
#if FSL_FEATURE_ADC_HAS_DMA
userConfigPtr->dmaEnable = false;
#endif /* FSL_FEATURE_ADC_HAS_DMA */
userConfigPtr->refVoltSrcMode = kAdcRefVoltSrcOfVref;
userConfigPtr->continuousConvEnable = true;
return kStatus_ADC_Success;
}
After that, customer need compile the lib and related demo projects, the ADC resolution will be changed.
Wish it helps.
best regards 
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Changing the KSDK's source file or rebuild the library is not necessary. ADC_DRV_StructInitUserConfig...() is provided for quick configuration. These would be an available group of setting, but may not fit the user's actually application. So the configuation structure of "adc_user_config_t " can be filled according to application manually by users. For example, if you want to just change the converter's resolution, just use the code like the following:
--------------------------------------------------
adc_user_config_t MyAdcConfigStructure;
ADC_DRV_StructInitUserConfigForIntMode(&MyAdcConfigStructure);
MyAdcConfigStructure.resolutionMode= kAdcResolutionBitOfSingleEndAs16;
ADC_DRV_Init(0U, &MyAdcConfigStructure);
...
--------------------------------------------------
Eventually, users can fill the "MyAdcConfigStructure" totally by their own without the API of ADC_DRV_StructInitUserConfig...().
All these work can be done just in Application Layer and do not have to change the KSDK.
May the illustration help you.
Best regards!
Andrew SU
8/25, 2014