KSDK Power manager

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSDK Power manager

1,653件の閲覧回数
andersbergström
Contributor II

Hi,

 

We are currently using KSDK 1.0 with KDS 1.1.1. The application uses FreeRTOS.

 

To set the application into mode with power manager, mode: kPowerManagerVlps is no problem.

 

However, we want to wake up the application, either via CAN or Ethernet.

When reading the reference manual for the K64, the wake-up method seems

to be interrupt. Do we need to set the system back into mode: kPowerManagerRun and where do we

place the function call for that?

 

Best regards,

Anders

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,414件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Anders,

Seems CAN can wake the system up from VLPS mode, so it should be no problem to use CAN module as the wakeup source under VLPS mode, please kindly refer to the following for details.

1.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,414件の閲覧回数
andersbergström
Contributor II

Alright, thanks!

We will fully test this during the system integration phase.

Best regards,

Anders

0 件の賞賛
返信