KSDK Clock Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KSDK Clock Configuration

跳至解决方案
2,564 次查看
guillaumetiffin
Contributor III

Hello,

 

I'm facing a problem with the KSDK V1.3.

I was using the MQX V4.0 and V4.1 with a k60FX512VLQ15 144 pin

 

I have a quartz of 32Khz for the RTC and an oscillator of 50MHZ on the pin PTA18.

 

With my previous version of MQX, no problem to start the MCU.

 

With the KSDK V1.3, I can succeed to start the MCU.

I'm always locked in the function "CLOCK_HAL_SetPbeMode" at the line "while (!CLOCK_HAL_IsPll0Locked(base)) {}"

 

You can find in attachement a part of the schematic with the connection of the 50 MHz quartz.

 

How can I do to tune the clock to succeed to run an app?

 

I took the code of the K60D10 as an example.

 

Can you help me with this issue?

 

Regards,

 

Guillaume

标签 (1)
0 项奖励
回复
1 解答
2,388 次查看
guillaumetiffin
Contributor III

Hi,

In fact I searched for more informations about my issue.

I decided to enter in the details of the initialization procedure.

In fact the K60FX series is not supported by the KSDK.

For me it's not a really good news and I'm worried about the future for my board because I can't have the new evolution of the KSDK.

Regards,

Guillaume

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,388 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Guillaume,

I apologize for the late response. Please, is the issue still actual for you?

Please, have you tried any KSDK demo? For example web_hvac demo, which uses 50 MHz external crystal or do you have custom code or what is your initialization?

Thank you.

Best Regards,

Iva

0 项奖励
回复
2,389 次查看
guillaumetiffin
Contributor III

Hi,

In fact I searched for more informations about my issue.

I decided to enter in the details of the initialization procedure.

In fact the K60FX series is not supported by the KSDK.

For me it's not a really good news and I'm worried about the future for my board because I can't have the new evolution of the KSDK.

Regards,

Guillaume

0 项奖励
回复