KSDK C++ Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,923件の閲覧回数
kalden_srcinc
Contributor IV

I have posted before that the header files of the KSDK do not mesh well with cpp source files compiled against them.  Is there any chance of this getting corrected in the next release?

 

I was able to put together a patch that resolves at least the issues I have run into.  I haven't compiled in every source file, so I'm sure this is not complete.  The KSDK code has carriage returns in it, so you need to use --binary when running patch.

Original Attachment has been moved to: ksdk_cpp.patch.zip

ラベル(1)
0 件の賞賛
返信
1 解決策
1,741件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Kevin,

I got the information that the issue was resolved in coming KSDK release.

Best Regards,

Iva

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,742件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Kevin,

I got the information that the issue was resolved in coming KSDK release.

Best Regards,

Iva

0 件の賞賛
返信
1,741件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Kevin,

thank you for the interest and your solution. I transmit it to SDK development team.

Have a nice day,

Iva

0 件の賞賛
返信