KSDK_1.3.0 DSPI issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KSDK_1.3.0 DSPI issue

982 次查看
carlossilva
Contributor I

Hello, im using SPI and the fsl_dspi official driver, I noticed that when I used DSPI_MasterTransferBlocking function, i got an unhandled interrupt .

 

Here is my setup: KSDK_1.3.0 board: frdmk64f.

标签 (1)
0 项奖励
回复
1 回复

902 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Carlos,

After the unhandled interrupt occurs, pls check the interrupt source index in the xpsr in debugger of the tools you are using, the bit0~8 of xpsr register represent the interrupt source index.

If the interrupt source index is 3(hard fault interrupt), it is a bit complicated, for example you use a peripheral whose clock is not enabled, or you access a memory which does not exist, all of the case can lead to hardware fault interrupt.

Anyway, i suggest you download SDK2.0 package from the link:

http://www.nxp.com/ksdk

Hope it can help you

BR

Xiangjun Rong

0 项奖励
回复