KSDK 1.0.0 Demos with TWR-K64F-120M

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KSDK 1.0.0 Demos with TWR-K64F-120M

1,047 次查看
jayhodkinson
Contributor I


Not sure of the best place to post this but trying to build the example code for the KSDK 1.0.0. I get the following attached error. KDS is 1.1.1.

I can build my test code and run it on the board so not sure what I am missing for the example code.

Original Attachment has been moved to: error.txt.zip

标签 (1)
0 项奖励
回复
2 回复数

913 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Jay:

The error implies that you have not compiled the KSDK platform library for K64.

To do this check the instructions in the Kinetis SDK K64 User's Guide.pdf in your KSDK installation:

C:\Freescale\KSDK_1.0.0\doc\Kinetis SDK K64 User's Guide.pdf

Refer to Appendix A, disregarding IAR and Keil parts and only pay attention to KDS instructions.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

913 次查看
jayhodkinson
Contributor I

Hello Jorge

That was it. I got it build and running on the board.

Thank you

Jay

0 项奖励
回复