KL03Z enters unknown state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL03Z enters unknown state

Jump to solution
1,594 Views
gnichimohamed
Contributor III

Hello

I have a custom pcb made out of KL03z microcontroller. I was debugging my application quite ok then suddenly the board is not debuggable anymore. I am using segger jlink to debug my app, flashing works ok but the program starts not in main.152542_152542.PNGdebug.PNG

As soon as i pause the debugging, things get weird.

152546_152546.PNGdebug2.PNG

Thanks for any help

Labels (1)
0 Kudos
Reply
1 Solution
1,442 Views
gnichimohamed
Contributor III

it turned out to be an nmi_b interrupt that's causing  the problem. I had one pot at that pin, if the pot is low, that will cause an interrupt which stops everything. I had to disable the nmi interrupt from flash.

View solution in original post

0 Kudos
Reply
4 Replies
1,442 Views
DavidS
NXP Employee
NXP Employee

Hi Gnichi,

Try removing all breakpoints and try again.

https://mcuoneclipse.com/2014/10/11/failed-to-debug-with-gdb-breakpoints-or-expressions-on-non-exist...

Regards,

David

1,442 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Maybe reloading the KDS tools/powering off/on the chip can make it work.

Regards

xiangjun Rong

0 Kudos
Reply
1,442 Views
gnichimohamed
Contributor III

Thank you guys for the answers, it seems that weird issues keep coming.

After two days leaving the boards, they are back working normally, i don't know what happened

0 Kudos
Reply
1,443 Views
gnichimohamed
Contributor III

it turned out to be an nmi_b interrupt that's causing  the problem. I had one pot at that pin, if the pot is low, that will cause an interrupt which stops everything. I had to disable the nmi interrupt from flash.

0 Kudos
Reply