K81 SDK availabe?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K81 SDK availabe?

1,941 Views
izmile
Contributor III

Hi,

 

I am trying to find the header file and driver library for K81 MCU. Can some one point me at the right direction?

I could get the K82 SDK but not the K81. 

 

Thanks,

-Ismail

Labels (1)
0 Kudos
Reply
2 Replies

1,796 Views
izmile
Contributor III

Thanks Xiang.

Yes, I was proceeding with the K82 SDK but then I just got the TWR-POS-K81 reference design which had what I need. We got this reference design after an NDA.

Thanks,

-Ismail

0 Kudos
Reply

1,796 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Mohamed,

Yes, we have not developed the SDK for K81. I have not found out the K81 header file either. i tried to create a project based on K81, but the KDS tools has not option to select K81.

Currently, I suggest you use K82 or SDK based on K82 to develop project for K81, it seems that the main difference between K81 and K82 is that K81 has tamper module.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply