K81+LPUART+FreeRTOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K81+LPUART+FreeRTOS

1,506 Views
lakshmikandhanp
NXP Employee
NXP Employee

I am new to Kinetis and K8x series. I am using a twrk81f150m board and trying to do a simple uart send/Receive with a PC side Application.facing an issue of Receive not more than 8 bytes on twrk81 .But the Send process works fine and able to receive more bytes in PC app (Teraterm).

i am using the below API for the uart communication .

LPUART_ReadBlocking(DEMO_LPUART,RxBuffer,32); 

where #define DEMO_LPUART LPUART1

Please let me know,what am i doing wrong here.

Is there any sample app ,i can refer for LPuart usage .

 

Thanks

LK

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,306 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have tested the example located at:

C:\Freescale\SDK2.0_K82\boards\frdmk82f\rtos_examples\freertos_lpuart\kds

I do not think there is any issue. You can transfer a file from Hyperterminal or the other tools and check the characters you received in the tools.

Can you tell me the tools you are using to transfer message and the screenshot of the receiver in the tools?

BR

XiangJun Rong

0 Kudos
Reply