K22 USB CDC sample code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K22 USB CDC sample code

2,714 次查看
isaotakashima
Contributor IV

I'm looking forward to the USB CDC sample code for the K22.

Does Kinetis SDK include this sample code?

Is that sample code working on the TWR-K21F120M tower board?

Please advise as soon as possible.

 

Best regards,

Takashima

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,683 次查看
trytohelp
NXP Employee
NXP Employee

Hi Takashima,

Under the KSDK installation there is a folder \KSDK_1.0.0\usb\

I recommend you to have a look in the \KSDK_1.0.0\usb\doc manuals.

An example for CDC is available under \KSDK_1.0.0\usb\example\host\cdc.

Depending of the development tool used you must follow the right process defined in the manual:

    \KSDK_1.0.0\usb\doc\Integration of the USB Stack and Kinetis SDK.pdf

For KDS (probably true for other dev tool) I see there are examples for FRDM-K22, FRDM-K64, TWR-K22F120M, TWR-K64F120M.

Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复