K22 USB CDC sample code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K22 USB CDC sample code

2,726件の閲覧回数
isaotakashima
Contributor IV

I'm looking forward to the USB CDC sample code for the K22.

Does Kinetis SDK include this sample code?

Is that sample code working on the TWR-K21F120M tower board?

Please advise as soon as possible.

 

Best regards,

Takashima

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,695件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Takashima,

Under the KSDK installation there is a folder \KSDK_1.0.0\usb\

I recommend you to have a look in the \KSDK_1.0.0\usb\doc manuals.

An example for CDC is available under \KSDK_1.0.0\usb\example\host\cdc.

Depending of the development tool used you must follow the right process defined in the manual:

    \KSDK_1.0.0\usb\doc\Integration of the USB Stack and Kinetis SDK.pdf

For KDS (probably true for other dev tool) I see there are examples for FRDM-K22, FRDM-K64, TWR-K22F120M, TWR-K64F120M.

Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信