Issues with freeRTOS tickless on K21

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues with freeRTOS tickless on K21

13,383 Views
martis
Contributor II

I am using freertos in my application, and I am now trying to lower the power consumption by implementing tickless mode.

 

However, I have some issues regarding the implementation of vPortSuppressTicksAndSleep.

 

I used the freertos_tickless_twrk21f120m project from SDK_2.0_TWR-K21F120M as a starting point. As it is, the example seems to be working, but when starting to modify it and test other frequencies, it does not behave as expected.

 

The LPTMR is setup with the default config which means 1khz clock.
However, configLPTMR_RATE_HZ is set to SystemCoreClock, which is 120000000.
When calculating the amount of LPTMR counts for one tick, the following expression is used:

 

ulLPTimerCountsForOneTick = configSYSTICK_CLOCK_HZ / configLPTMR_RATE_HZ;

 

As these two are defined to be the same, ulLPTimerCountsForOneTick is one. In the example  both configTICK_RATE_HZ and configLPTMR_RATE_HZ is 1000, which means that it is correct that one tick is 1 tick on the LPtimer.
But for the general case, the calculation doesn't make any sense, as the it doesn't include anything about the tick rate.

 

The correct calculation should be:
ulLPTimerCountsForOneTick = configLPTMR_RATE_HZ / configTICK_RATE_HZ;

 

Fixing this issue allows me to play with different frequency settings of the LPTimer and RTOStick, and the timing looks correct.
But this is only until the sleep period is interrupted by an external interrupt, which sometimes causes the project to hang. This is due to the
vTaskStepTick( ulCompleteTickPeriods );
which is called with
ulCompleteTickPeriods = LPTMR_GetCurrentTimerCount(TICKLESS_LPTMR_BASE_PTR);
as parameter.

 

This again assumes that the LPTMR is at the same frequency as the rtos tick.

 

Adding:
ulCompleteTickPeriods /= ulLPTimerCountsForOneTick;
after reading out the value scales the value correctly, and avoids getting caught in the configASSERT in vTaskStepTick due to wrong input.

 

I do not know if there are any more errors in this implementation, so it would be great if someone could have a look at this.

Labels (1)
23 Replies

1,021 Views
2bluesc
Contributor II

Any updates? I'm running to the same problem on the Cortex-M0 port.

0 Kudos
Reply

1,021 Views
javiercardona
Contributor III

I also happen to have the same problem on the Cortex-M0 (KL27).

0 Kudos
Reply

1,021 Views
soledad
NXP Employee
NXP Employee

Hi,

Just wanted to let you know that I’m already working on your issue.I will get back to you know as soon as possible.


Have a great day,

Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply