Is there any tool like PE in SDK 2.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any tool like PE in SDK 2.0?

1,349 Views
zhongshen
Contributor III

I have used PE with SDK 1.3 with KDS 3.0, so that it is easy to add the component to the project and configure the pins and initiate the component, let me to focus the program of application. And now there is KDS 3.2 and SDK 2.0, but there is not PE support. I need to study the datasheet and understand the registers on the component to initiate the pinmux and set the registers.

 

Is there any tool like PE in SDK 2.0  to make program easy?

 

Thanks.

 

Zhong Shen

Labels (1)
0 Kudos
Reply
4 Replies

1,097 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Zhong Shen,

we prepared configuration tools, which will be available soon.

I will keep you informed,

Best Regards,

Iva

0 Kudos
Reply

1,097 Views
zhongshen
Contributor III

Hi Iva,

Any update?

0 Kudos
Reply

1,097 Views
ivadorazinova
NXP Employee
NXP Employee

Hello,

no, these tools are no available just now. But it will be ready soon.

You will see it under Tools in kex.freescale.com

tools.png

At the moment is available Power Estimation Tool.

I will keep you informed.

Have a nice day.

Iva

0 Kudos
Reply

1,097 Views
zhongshen
Contributor III

Thanks.

0 Kudos
Reply