Is lwIP MISRA Compliant MCUXpresso SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is lwIP MISRA Compliant MCUXpresso SDK

2,489 Views
abdullahshafiq
Contributor I

Hello,

         I have gone through the MCU Xpresso SDK manual. It is stated that the start code and drivers are MISRA compliant. I wanted to ask that whether the optional middle ware(lwIP) is MISRA compliant or not. If it is compliant, then is it 2004 or 2012.The board I am using in FRDM-K64F and my application requires a TCP/IP Stack but also requires MISRA Compliance. Any help will be highly appreciated. 

Regards,

Abdullah Shafiq

Labels (1)
0 Kudos
Reply
1 Reply

2,276 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Abdullah Shafiq 

No,  only  code we developed as a part of MCUSDK – drivers and USB stack are MISRA compliant.  3rd party code such as LWIP is not.


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------