Is lwIP MISRA Compliant MCUXpresso SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is lwIP MISRA Compliant MCUXpresso SDK

2,486件の閲覧回数
abdullahshafiq
Contributor I

Hello,

         I have gone through the MCU Xpresso SDK manual. It is stated that the start code and drivers are MISRA compliant. I wanted to ask that whether the optional middle ware(lwIP) is MISRA compliant or not. If it is compliant, then is it 2004 or 2012.The board I am using in FRDM-K64F and my application requires a TCP/IP Stack but also requires MISRA Compliance. Any help will be highly appreciated. 

Regards,

Abdullah Shafiq

ラベル(1)
0 件の賞賛
返信
1 返信

2,273件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Abdullah Shafiq 

No,  only  code we developed as a part of MCUSDK – drivers and USB stack are MISRA compliant.  3rd party code such as LWIP is not.


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------