Is K22 build target compatible with K21?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is K22 build target compatible with K21?

2,702件の閲覧回数
francescosalvat
Contributor II

Hi all,

I want to use mbed libraries on MK21DN512VLK5 microcontroller but there isn't a ready-to-use target yet. Checking on documentation and SDK seems that the only differences beetween K22 and K21 are security features, so can i use the build target for K22 to build for K21? How can i extend it to support RNG, HW encryption and Tamper detection?

 

Thank you.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,571件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Francesco,

no, because MK22DN512VLK5 and MK21DN512VLK5 has two different processors.

Best Regards,

Iva

0 件の賞賛
返信

2,571件の閲覧回数
francescosalvat
Contributor II

Ok, and what are the differences beetween them?

Reading docs and comparing SDK files seems that are equals except for security implementations (CAU and RNG).

Thank you!

0 件の賞賛
返信

2,571件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Francesco.

KSDK supports K22 devices with cpu frequency 100 MHz and 120 MHz.

Please, take a look at the attached guide.

Best Regards,

Iva

0 件の賞賛
返信