Interrupt based LP UART driver 

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interrupt based LP UART driver 

4,203件の閲覧回数
anilnadargi
Contributor II

Hi ,

We are working KL27 series SOC . We are using LPUART module for one of peripehrial .

We need to implement the in the LPUART module in interrupt mode i.e. if some data arrived at the LPUART buffer ,

interrupt for LPUART will be raised .

 

We have done with adding the LPUART component with following configuration

a. Enabled the RX interrupt .

b. Enabled the RX callbacks with user buffer as "char bufferr[500]" .

c. Toggle the LED in the RX Callback .

 

Currently the RX callback is called for each byte . So if the peripheral is sending multiple data bytes we are receiving multiple interrupts .

 

Our expectation is to call the RX callback function when the data buffer is full i.e. if at least 500 bytes are received by LPUART .

We also checked the Component configuration in the KDS but there is no such configuration to set the buffer size for triggering the RX callback.

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,517件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Anil,

Regarding your question, I suppose you use the KSDK2.0 for Kl27, if you use the LPUART_TransferReceiveNonBlockin() function, the LPUART uses interrupt mechanism to transfer data.

You can refer to the example:

C:\KSDK2.0_KL27\boards\frdmkl27z\driver_examples\lpuart\interrupt_transfer\kds

In the code,  if you hope the callback() is called after 500 bytes have been received, you can change the example:

receiveXfer.data = g_rxBuffer;

    receiveXfer.dataSize = 500; //ECHO_BUFFER_LENGTH; Rong modified

    while (1)

    {

        /* If RX is idle and g_rxBuffer is empty, start to read data to g_rxBuffer. */

        if ((!rxOnGoing) && rxBufferEmpty)

        {

            rxOnGoing = true;

            LPUART_TransferReceiveNonBlocking(DEMO_LPUART, &g_lpuartHandle, &receiveXfer, NULL);

        }

The receiveXfer.dataSize specifies the received number of bytes, after the number of bytes has been received, the callback function  LPUART_UserCallback() is called.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

3,517件の閲覧回数
anilnadargi
Contributor II

Hi Thanks Rong for your inputs .

So you mean the system will receive interrupt for each byte receiption as the KL27 SOC contains only 1 byte ( 8-bit ) data register.

Is there any way to configure the LPUART to generate interrupt for every 500 bytes ( as our example ) of reception .

Thanks ,

Anil N.

0 件の賞賛
返信

3,517件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Anil,

There are two mode for LPUART receiving:interrupt mode or polling mode, polling mode means that you poll a flag in LPUART status register which indicates if it has received byte, but the polling mode is inefficient. Interrupt mode means that an interrupt is invoked once the LPUART receives a byte, for the SDK, in the ISR, the code read the received data to memory, check if the predefined number of bytes has been received, if it has received the predefined number of bytes, the callback(0 function is called.

Hope it can help you.

BR

XiangJun Rong

0 件の賞賛
返信

3,517件の閲覧回数
anilnadargi
Contributor II

Thanks XiangJun Rong for your inputs .

We moved from KDS 1.X to KSDK 2.0 version and using FreeRTOS LPUART driver APIs. But with the FreeRTOS LPUART driver I am getting below error .

Debug/../drivers/freertos_drivers/fsl_lpuart_freertos.c:62: undefined reference to `xTimerPendFunctionCallFromISR'

It seems to be issue in the FreeRTOS function not avaliable within the KSDK 2.0 .I have seen the configuration but no settngs for the same.

Please let me know how we can add this API in the FreeRTOS OS supported within the KSDK V 2.0.

Thanks ,

Anil N.

0 件の賞賛
返信

3,517件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Anil,

I think you do not include header file, which includes the prototype which leads to the issue.

BR

XiangJun Rong

0 件の賞賛
返信