Install New Software

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Install New Software

2,429 Views
guilhermebaggio
Contributor I

Efetuei o download do KSDK da FRDM-KL27Z e ao tentar instalar pelo Help > Install New Software recebo a seguinte mensagem: "No software site found at jar:file:C:/Users/Guilherme/Downloads/SDK_2.0_FRDM-KL27Z.zip!/". Como proceder?

Labels (1)
0 Kudos
Reply
3 Replies

2,199 Views
ivadorazinova
NXP Employee
NXP Employee

Guilherme Baggio,

Maybe information from readme file helps you:

Installation Instructions

1. Start Eclipse/Kinetis Design Studio

2. Select the menu Help > Install New Software

3. Click 'Add' button and type Name = "New Kinetis SDK 2.x Project Wizard", Location = select: NPWforKinetisSDK2x.zip

4. Confirm installation

5. Restart the IDE

Recommended Usage:

- To download SDK 2.0 package:

  1. Go to http://kex.nxp.com/ and click "Build an SDK"

  2. Create a new configuration: select processor or board

  3. Select SDK version 2.0 and "Kinetis Design Studio" as a toolchain

  4. Use the 'Build SDK Package' button to create the ZIP file

  5. Download the ZIP package and unzip it into a user folder

- To Create new project with the wizard:

  1. Start Kinetis Design Studio

  2. Select the menu File > New  > C Project

  3. Enter project name and select "Executable - Kinetis Project for SDK 2.x" and press [Next>]

  4. Select where you have unzipped the SDK package from previous step and press [Next>]

  5. Select board or processor and press [Next>]

  6. Finish wizard

- Now you can build and debug your project

Hope this helps.

Iva

0 Kudos
Reply

2,199 Views
lepol
NXP Employee
NXP Employee

Hi Guilherme,

first we need to know which version of SDK you use. If it is KSDK 1.3.0 then unpack the .zip and forward SDK_2.0_FRDM-KL27Z/tools/<exclipse_update/SDK_1.3.0_FRDM-KL27Z_1.0.0_Eclipse_update.zip> to the path. If it is a KSDK 2.0 then use the newest Kinetis Design Studio and select File -  New - KSDK 2.x project.

Best regards,

Lenka

0 Kudos
Reply

2,199 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Guilherme Baggio,

please have you installed update for KSDK 2.0?

I mean Help -> Check for Updates

KSDK_3.png

New Kinetis SDK 2.x Project Wizard and click on Next and install the update

KSDK_.png

after successful installation you will see Kinetis SDK 2.x Project Wizard in File -> New

KSDK_2.png

Please let me know, if you solve your issue.

Best Regards,

Iva

0 Kudos
Reply