INT_SYS_InstallHandler call stuck

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

INT_SYS_InstallHandler call stuck

2,511件の閲覧回数
sandeepthota
Contributor I

I am trying to install an interrupt handler for GPIO on K64 twr kit using KSDK 1.2.0. These are the steps I am following,

CLOCK_SYS_EnablePortClock(PORTE_IDX);
PORT_HAL_SetMuxMode (PORTE, 6, kPortMuxAsGpio );
GPIO_HAL_SetPinDir(PTE_BASE_PTR, 6, kGpioDigitalInput);
INT_SYS_InstallHandler(PORTE_IRQn, BSP_GPIO_IRQHandlerPortE);
PORT_HAL_SetPinIntMode(PORTE, 6, kPortDmaRisingEdge );
NVIC_SetPriority(PORTE_IRQn, 0);
INT_SYS_EnableIRQ(PORTE_IRQn);

But the call to InstallHandler is stuck, what could be the reason for this?

0 件の賞賛
返信
1 返信

2,031件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sandeep Thota,

  KSDK1.2 is very older, please download the newest KSDK2.1-TWR-K64F120M code from this link:

Welcome to Kinetis Expert | Kinetis Expert

Click build an SDK, and choose the board as TWR-K64F120M, generate the code and download it.

We can modify the SDK_2.1_TWR-K64F120M\boards\twrk64f120m\driver_examples\gpio\input_interrupt

Add PTE6 input falling interrupt code:

void PORTE_IRQHandler(void)
{
  GPIO_ClearPinsInterruptFlags(GPIOE, 1U << 6);
  g_ButtonPress = true;
}

In main function:

    gpio_pin_config_t pte6_config = {
        kGPIO_DigitalInput, 0,
    };

    PORT_SetPinInterruptConfig(PORTE, 6, kPORT_InterruptFallingEdge);
    EnableIRQ(PORTE_IRQn);
    GPIO_PinInit(GPIOE, 6, &pte6_config);

Then, after you pull down the PTE6, you will enter the PTE6 handler.

pastedImage_1.png

I also attach the gpio_input_interrupt.c for your reference, you can unzip it to folder : SDK_2.1_TWR-K64F120M\boards\twrk64f120m\driver_examples\gpio\input_interrupt

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信