I need a FreeRTOS Reference Manual for v8.2.3.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I need a FreeRTOS Reference Manual for v8.2.3.

2,362件の閲覧回数
rogerchaplin
Contributor II

I'm starting development on a new project with KSDK 2.0, used the KSDK builder to create the SDK download. It comes with FreeRTOS v8.2.3 bundled. However, on the FreeRTOS website the only documentation I can find is for v9.0.0 which has some significant changes. Did somebody at Freescale/NXP tuck away a copy of the v8.2.3 reference manual they'd be willing to share? And knowing the tendency of Real Time Engineers, Ltd. to hide away old versions of documentation, wouldn't it make sense to bundle the correct version of the FreeRTOS reference manual along with the "Getting Started with KSDK and FreeRTOS OS" document when you build the KSDK for download?

タグ(2)
0 件の賞賛
返信
1 返信

1,938件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Roger,

It seems that you can download the version 8.2 of FreeRTOS RM from the link:

http://www.freertos.org/Documentation/FreeRTOS-Reference-Manual-Table-of-Contents.pdf 

Pls have a try

BR

Xiangjun Rong

0 件の賞賛
返信